Contact Mouser (International)  +49 (0)89 520 462 110     |     Feedback         
    
Cart  
 |    Change Country  Change Location  USD
 
Mouser International Mouser International

Incoterms: DDP is available to customers in EU Member States.
All prices include duty and customs fees on select shipping methods.


Incoterms: DDU applies to most non-EU customers.
Duty, customs fees and taxes are collected at time of delivery.

Please confirm your currency selection:

US Dollars
USD is accepted in all countries.

Other currency options may also be available - see
Mouser Worldwide.
Home » Applications & Technologies » Audio Applications Electronics
Applications & Technologies
Amplifiers
Audio Amplifiers

 Audio Amplifiers are designed to increase the amplitude of a small input signal while maintaining the linearity of the original signal. In other words, the detail and characteristics of the original signal will be maintained. The audio amplifier market has seen many changes, resulting in a wide selection of amplifier ICs available to design engineers.

Audio amplifier ICs are now available to address specific applications with a certain amplifier class and number of channels. Audio amplifiers are available in single channel (mono), two-channel (stereo), or multi-channel amplifiers that may support 6 or more channels of high quality audio. Various classes are used to differentiate between amplifier types for audio applications:

» View Audio Amplifiers

Audio & Video Connectors
Audio & Video Connectors

When transmitting audio or video signals over any distance, the connectors are potentially the most fragile part of the signal path. Paying attention to these seemingly mundane devices can pay major dividends in terms of signal integrity and product reliability. Many analog audio and video connections use standard RCA connectors, sometimes referred to as “phono connectors.” RCA connectors are commonly used in consumer audio applications such as connections for component hi-fi systems, but are also frequently used for IEC 60958 Type II (S/PDIF) digital audio signals.

» View Male Phone Connectors

» View Female Phone Connectors

» View Loudspeaker Connectors

» View Male XLR Connectors

» View Female XLR Connectors

» View HDMI, Displayport & DVI Connectors

» View RCA Phono Connectors

» View DIN Connectors

» View Patch Panels

Data Converters
Audio Data Converters

If you want to do any digital processing with analog audio you’ll need to convert your analog signals into the digital domain using Audio Data Converters. As their names imply, Audio A/D Converters convert signals from the analog world into the digital domain and after processing Audio D/A converters will convert the digital signals back to the analog domain. There are different types of data converters, but the key specs to compare in audio applications are their resolution (number of bits) and the sampling rate. These specification will affect the dynamic range which should be pre-determined as part of your design. Compact discs provide high quality music (20 Hz to 20 kHz) are sampled at 44.1 kHz with 16-bit precision. High resolution audio more commonly uses 24-bit resolution with samples rates of 192 kHz or more. On the other end of the spectrum, telephone quality speech (200 Hz to 3.2 kHz) can be sampled at 8 kHz with 12 bit precision.

» View Audio A/D Converters

» View Audio D/A Converters

» View Audio CODECS

» View Audio Sample Rate Converters

Development Tools
Audio Development Tools

Evaluation boards let you quickly determine just how well the audio processor that looked good on the datasheet will perform in your pending design. Full development kits go even further and include a wide range of on-board peripherals, application programming interfaces (APIs), reference designs, firmware, software libraries, sample source code, user interfaces, and a serial or USB connection to connect the development kit hardware to a PC host. With a development board you can quickly prototype, test, and debug your design, eliminating the time and cost involved in developing a series of prototype boards.

Development boards typically come with either an onboard debugger or a separate debugger and an onboard debug interface. Check the software library for functions and filters that can be useful in audio applications—they can save a good deal of programming time and effort. Development kits pay for themselves (and more) in terms of shortened development time and avoidance of errors in the design process.

» View Audio IC Development Tools

Indication & Alert
Indication & Alert

When an event occurs that requires attention there are two ways to generate an alert: sight and sound. Usually an LED lights up and an audible alarm sounds. The audio alert can be anything from the buzzer on a cell phone to a resonant voice that announces, “I’m sorry Dave, I’m afraid I can’t do that.”

Audio alert devices are simple electromechanical transducers that span a tremendous range of technologies (buzzers, horns, strobes, sirens, tone generators), tones (chirps, chimes, beeps, whoops, and warbles), frequencies (6.3-9100 Hz), volumes (6-127 dB), and voltage ratings (0.1-220V). With so many audio indicators, there is bound to be an appropriate device available for any given application.

Product selection is very much application driven. How loud does it need to be? How immediate is the need for attention? A buzzer may be sufficient to alert the person in the next room that the dryer load is finished; but a smoke detector will need to issue a piercing alarm. When an event occurs that requires attention and it’s not safe to assume that someone will quickly see a visual alert, an audio alert or alarm should be a required part of the system design.

» View Indication & Alert Products

Microphones and Preamplifiers
Microphones and Preamplifiers

Amplifying the output from a microphone enough to fill a large auditorium requires a great deal of gain. In order to obtain the best possible signal-to-noise ratio (SNR) it’s imperative to amplify the microphone’s output as quickly and cleanly as possible. If you start with a noisy signal, no amount of downstream filtering will give you a satisfactory result.

Microphone preamplifier ICs are specialized amplifiers that provide high gain, low noise, low distortion, and—if embedded in the microphone—low power; their characteristics are dictated by the type of microphone.

» View Microphones

» View MEMS Microphones

» View Microphone Preamplifiers ICs

Potentiometers
Audio Potentiometers, Trimmers & Rheostats

Potentiometers (Pots) are variable resistance devices commonly used as the interface to control various features in audio products. They are simple but important devices that allow you to dial in the desired amount of resistance which may affect volume, tone or other aspects of the audio signal. Typically pots are analog devices but digital pots that mimic the behavior of their analog counterparts are also available. Potentiometers come in rotary or slide panel packages with various sizes, shaft configurations and tapers, and can be found in products designed for the pro audio, consumer, portable and automotive markets.

» View Audio Potentiometers, Trimmers & Rheostats

Processors
Audio Processors

Audio signals almost invariably require processing, whether to filter out noise, remove echoes, reduce distortion, optimize frequency response, or compress them for transmission or storage. Audio signal processors offer a variety of tools to assist in optimizing sound for audibility, intelligibility, and fidelity. In commercial audio applications, audio signal processors are typically employed within or just after the mixing stage, but before amplification.

Audio signal processors generally fall into one of two categories: Audio SoCs—integrating multiple digital audio management features into a single, complex package—and audio DSPs, which range from hardware implementations of specific codecs to fully programmable DSPs. Audio DSPs are available with a wide range of features, so you can select the feature set to match design requirements.

» View Audio SoCs

» View Audio DSPs

Speakers & Transducers
Speakers & Transducers

Speakers are electromechanical transducers that convert an audio signal to audible sound, the opposite of microphones, with which they share many of the same characteristics. Like microphones, there different types of speakers.

The smallest speakers, if you can call them that, are the electret transducers used in hearing aids. Marvels of miniaturization, they include an electret microphone, programmable DSP processor, audio amplifier, and electret audio output device, all of which must work for days off a tiny zinc-air battery. The electret transducer makes that possible. Earbuds are the next step up in size, but they don’t face the same power constraints as hearing aids. They’re typically dynamic speakers, with a very small coil attached to a moving diaphragm. Larger headphones use the same design, though high-end ones may use electrostatic drivers that are essentially condenser microphones in reverse, with an electrically charged plate suspended between two perforated metal electrodes to which the audio signal is applied. Electrostatic speakers are more linear than moving coil designs and produce very crisp sound. The downside is they require a relatively high voltage power supply and they can’t move enough air to reproduce low frequencies well.

» View Speakers & Transducers

Transformers
Audio Transformer

While digital designers aren’t used to seeing transformers, they’re very useful in audio applications for isolation and impedance matching, both of which can be accomplished at the same time. Audio power amplifiers connect to 8-ohm loads, which is far lower than the output impedance of the amplifier. An output transformer matches the impedances and isolates the speaker from the amplifier’s collector or plate voltage.

When evaluating audio transformers it’s important to consider the impedance, power rating, isolation voltage, and frequency range. If the transformer will be operated near an RF or other EMI source, shielding may be necessary. Shielding shouldn’t be an issue with a low-impedance audio output transformer, but it definitely could be with a transformer feeding a high-impedance, high-gain input stage; in that case the transformer should be placed as close to the input jack as possible and far away from noise-emitting sources, for which its windings could act like an antenna.

» View Audio Transformers

Transmitters, Receivers, Transceivers
Transmitters, Receivers, Transceivers

Analog audio can move readily from a microphone to an amplifier as long as the cable and connectors are shielded and in good repair. But audio that needs to travel to a remote site with some distance needs to be digitized, encoded, transmitted, decoded, and converted back to analog at the far end. The audio transmitter accepts audio, channel status, and user data, which is then multiplexed, encoded, and driven onto a cable; at the receiving end the audio receiver does the reverse. This is clearly a more complicated task than moving analog sound a few feet over a microphone cord.

Digital audio is rarely transmitted raw—it’s always compressed and later decompressed by a codec. The choice of codec depends on how much signal loss can be tolerated due to compression and how noisy the signal path is liable to be. Audio transmitters usually contain ADCs and hardware-based codecs; receivers are just the reverse; and transceivers contain the essential elements of both.

» View Audio Transmitters, Receivers, Transceivers

Test Equipment
Test Equipment

Several types of test equipment can be used to capture and measure audio signals. The simplest test involves putting a single audio tone (usually 1 kHz) through the audio system and measuring the output with an oscilloscope and distortion analyzer, determining the acceptable input level before achieving an unacceptable level of total harmonic distortion (THD), which usually occurs just before clipping. Sweeping the input frequency will indicate the system’s bandwidth (+/- 3 dB).

Specialized audio signal generators can generate signals ranging from a short impulse, a burst, or a continuous signal. The signal can be a standard shape (pulse, ramp, sine wave, etc.), a sweep of frequencies, a controlled amount of noise, or an arbitrary waveform.

» View Audio & Video Test Equipment

Block Diagrams

DIGITAL RADIO

COMPRESSOR/ LIMITER

SOUNDBAR

NOISE CANCELLATION

WIRELESS HEADPHONES

GUITAR WIRING



REPLACEMENT PARTS

VINTAGE REPLACEMENT PARTS

Learn More About the TI TAS5548/58
TI - PCM5242 Audio Stereo
Differential-Output DACs

Excellent dynamic performance and improved jitter tolerance. A fully programmable miniDSP allows integration of filters, dynamic range controls, custom interpolators and other differentiating features.
Learn More About the Texas Instruments PCM5242 Audio Stereo Differential-Output DAC8
Learn More About STMicroelectronics MP23AB02B MEMS Digital Microphones
STMicroelectronics MP23AB02B MEMS
Digital Microphones

The MP23AB02B is a compact, low-power microphone with a low-profile MEMS sensing element that is capable of detecting acoustic waves and has an acoustic overload point of 125 dBSPL with a 64 dB SNR.
Learn More About STMicroelectronics MP23AB02B MEMS Digital Microphones
Learn More About Analog Devices ADAU145x SigmaDSP Digital Audio Processors
Analog Devices ADAU145x SigmaDSP
Digital Audio Processors

Analog Devices ADAU145x SigmaDSP Digital Audio Processors are optimized for efficient audio processing and automotive-qualified. The DSP core executes full programs while consuming only a few hundred mW of power.
Learn More About Analog Devices ADAU145x SigmaDSP Digital Audio Processors
Learn More About Switchcraft XLR Connectors
Switchcraft Sealed XLR
Connectors

These unique sealed XLR panel connectors are sealed to IP68 when unmated and mated pairs are sealed to IP66. Ideal for outdoor audio solutions.
Learn More About Switchcraft XLR Connectors
Learn More About Silicon Labs Si468x Single-Chip Digital Radio Receivers
Silicon Labs Si468x
Single-Chip Digital Radio Receivers

The Si468x family provides revolutionary advances in size, power consumption, and performance to enable high-volume, cost-sensitive multimedia products to incorporate digital broadcast features.
Learn More About Silicon Labs Si468x Single-Chip Digital Radio Receivers
Learn More About Bluegiga WT32i Bluetooth Audio Module
Bluegiga WT32i
Bluetooth Audio Module

WT32i Bluetooth 3.0 audio modules feature excellent RF performance and enhanced audio features. A DSP, stereo audio codec, and battery charger make it ideal for fixed and portable audio applications.
Learn More About Bluegiga WT32i Bluetooth Audio Module
More Featured Products
Switches
E-Switch Illuminated Rocker SwitchesLearn More
E-Switch Rocker SwitchesLearn More
E-Switch Illuminated Tactile SwitchesLearn More
Capacitors
Nichicon - Audio CapacitorsLearn More
Vishay - Tantalum CapacitorsLearn More
AVX - Audio F95 Conformal Coated TantalumLearn More
CDE - 225P Orange Drop CapacitorsLearn More
CDE - 715P Orange Drop CapacitorsLearn More
Nichicon - Audio CapacitorsLearn More
Semiconductors
TI - TAS5548/58 8-Channel HD Audio ProcessorsLearn More
ADI - ADAU1452 SigmaDSP Digital Audio ProcessorLearn More
Cirrus Logic - CS53L30 Ultra Low Power 4-Channel Microphone A/D ConvertersLearn More
Fairchild - FSA550 4PST Depletion Mode Isolation SwitchLearn More
Cirrus Logic - CS4354 24-bit Digital to Analog ConverterLearn More
International Rectifier - IR43xxM Class D Audio AmplifiersLearn More
Maxim - MAX97200 Class H DirectDrive® II Headphone AmplifiersLearn More
Maxim - MAX98355/56 Class D Audio AmplifiersLearn More
Texas Instruments - TMS320C5515 Fixed-Point Digital Signal ProcessorsLearn More
Texas Instruments - PCM270xC USB Stereo Audio DACsLearn More
Connectors
Neurik - NP2X-AU-SILENT 1/4" silentPLUGLearn More
Switchcraft - XLR ConnectorsLearn More
Amphenol Audio - Audio ConnectorsLearn More
Neutrik - powerCON TRUE1 Connectors/td>Learn More
Switchcraft - DC Power Jacks and PlugsLearn More
Switchcraft - High Amperage Power Jacks and PlugsLearn More
Potentiometers
Bourns - Guitar Potentiometer Design KitsLearn More
Speakers
PUI Audio - Enclosed Loudspeaker ComponentsLearn More
DB Unlimited – Audio ComponentsLearn More

HOW TO TEST - AUDIO
Teledyne LeCroy ArbStudio Arbitrary Waveform Generator ArbStudio combines 125 MHz bandwidth with fast 1 GS/s sample rate and 16-bit resolution to meet the needs of today’s engineers with uncompromised performance and a wide variety of signal types and generation modes.
 
Automotive
 
Circuit Protection
 
Computer
 
Docks
 
General Audio
 
Headsets
 
Home Theater/Audio
 
Internet Phone
 
Mobile Phone
 
MP3 Player
 
Network Audio
 
Portable Device
 
Pro Audio
 
Radio
 
Tablet
 
Wireless
 
Amplifiers
 
Broadcast
 
Data Conversion
 
Digital Signal Processing
 
Interface
 
Noise Reduction
 
Passives
 
Potentiometers
 
Power Management
 
Signal Processing
 
Transducers & Speakers
 
Wire & Cable
 
Wireless
 
Application Note
 
Data Reference Design
 
Design Guide
 
Product Selector Guide
 
Seminar
 
Solutions Guide
 
Tutorial
 
Webcast
 
Webinar
 
White Paper
 
Analog Devices
 
Atmel
 
Belden
 
Bourns
 
Cirrus Logic
 
Fairchild
 
Freescale
 
International Rectifier
 
Knowles
 
Maxim
 
Microchip
 
MCC
 
Neutrik
 
ON Semi
 
PUI Audio
 
ROHM
 
Silicon Labs
 
ST
 
Switchcraft
 
Texas Instruments
 
THAT Corporation
 
Vishay
 
Wurth Electronics