Contact Mouser (International)  +49 (0)89 520 462 110     |     Feedback         
    
Cart  
 |    Change Country  Change Location  USD
 
Mouser International Mouser International

Incoterms: DDP is available to customers in EU Member States.
All prices include duty and customs fees on select shipping methods.


Incoterms: DDU applies to most non-EU customers.
Duty, customs fees and taxes are collected at time of delivery.

Please confirm your currency selection:

US Dollars
USD is accepted in all countries.

Other currency options may also be available - see
Mouser Worldwide.
Home » Applications & Technologies » Low Power Electronics
Applications & Technologies
MCUs
Low Power MCU

Few if any decisions can have more impact on the power profile of a new design than the choice of an MCU. Choosing between new “ultra-low-power” MCUs can be confusing. While low-power is important it’s low energy that really counts—which ultimately makes the choice of an MCU application specific. Here’s what to look for:

First, there is no commonly agreed upon definition of ultra-low-power. Thanks to Ohm’s Law reducing the core voltage results in a dramatic reduction in power; processor cores running at 0.9V are becoming increasingly common. Shrinking line geometries have enabled higher device densities but at the expense of higher leakage; in low-power sensor applications, where the MCU spends most of its time in sleep mode, leakage current may contribute more to overall energy consumption than a high active current, possibly making an older 90-nm MCU a better choice than the latest 20 nm design.

» View Featured MCUs for Low Power

Power Mangement ICs
Low Power Power Mangement ICs

Engineers have numerous tricks to minimize power consumption in solid-state devices: static and dynamic process temperature compensation; power gating; clock gating; reduced core voltage; voltage islands; dynamic voltage and frequency scaling; and a variety of power-down modes. Managing all these controls has gotten so complex that it’s generated a whole category of power management ICs (PMICs), some of which are customized for a particular MCU.

Almost all leading MCU vendors offer PMICs designed to work in conjunction with their processors. These PMICs are complete power management solutions that typically contain multiple independent voltage regulators that meet the supply requirements of a particular MCU family. PMICs may include linear (LDO) and switching regulators (buck/boost/or both) and controllers. They can also handle voltage sequencing, current limiting, and surge protection. Many are programmable.

As MCUs become more complex, power management is increasingly handled on-chip. This is a distinct advantage when different portions of the chip need to move quickly between numerous power-down modes. Dynamic voltage and frequency scaling is a complex function that is more easily handled on-chip.

» View Featured Power Management for Low Power

RF Devices
Low Power RF

With seemingly every portable device going wireless, the need for low-power wireless design has never been greater. While there are no simple answers, there are a number of things it’s important to keep in mind.

All things being equal, the less time spent transmitting RF the less power will be required. Low-power wireless sensor nodes wake up for a few microseconds each second, poll for data, transmit it in a short burst, and go back to sleep. Protocols such as Wi-Fi (802.11) that are constantly polling for streaming data consume a lot more power than say Bluetooth (802.15.1), which can be in active, sniff, hold, or park mode.

Low-power wireless protocols such as Bluetooth Low Energy, Texas Instruments’ simpliciTI, and Microchip’s MiWi use small software stacks designed for low data rate applications such as wireless sensor nodes. They’re designed for point-to-point communications but can also work in star networks. ZigBee, while low energy, can operate in ad hoc mesh networks where a central node may be unreliable or even lacking.

» View Featured RF Products for Low Power

Analog Devices
Low Power Analog

Low-power and analog at first glance don’t seem to go together. Class A op-amps consume correspondingly more power as the input voltage rises; and achieving a good SNR may result in relatively high current drain.

There are various ways around the problem: First replace Class A op-amps with rail-to-rail common mode Class AB op-amps, which are biased at small currents and thus dissipate less quiescent power. In doing so be careful that you can still provide sufficient gain and output power, maximizing gain while preserving an acceptable bandwidth and slew rate.

Digitize the signal as soon as possible. You can often use digital filtering to compensate for a weak analog signal that might otherwise be too close to the noise floor.

» View Featured Analog Products for Low Power

Memory ICs
Low Power Memory

While most of the low-power buzz has centered on MCUs, memory is often the real power hog.

Flash memory is very popular for temporary data storage, both on- and off-chip. Flash is fast, with one typical 16-Mbit multi-purpose flash memory chip displaying read access times of 70-90 nsec. While the 3 μA standby current is low, this spikes to 9 mA in Write mode. Moving a lot of data to flash memory can take a big bite out of a power budget. If data is moving to and from off-chip flash, the number of wait states needed to keep memory in sync with the MCU can have a similar impact. Basically, choose an MCU with as much on-chip flash as you’re likely to need. If possible choose one that can also handle memory accesses by peripherals without waking the CPU.

SRAM is widely used for cache memory in high-speed applications. It’s fast, non-volatile—at least while powered up—and relatively low power. Asynchronous DRAM is cheaper (1T vs. 6T) and faster, but it needs to be constantly refreshed, which argues against using it much in applications where the processor will be in standby-mode most of the time.

» View Featured Memory Products for Low Power

Interface Devices
Low Power Interface

Data interfaces are often dictated by the system into which a device will be connected—automotive applications may have a CAN, LIN, FlexRay, or MOST interface; computers, USB or Ethernet; other embedded devices may communicate by I2C, UART, SPI, or a host of other protocols. The environment dictates the architecture; the power requirement is a secondary consideration.

But this needn’t always be the case. Protocols that continually poll other devices on the bus will draw far more power than those that wait for a signal or event. USB 2.0, for example, continually polls every device on the network to see if any one of them wants to send data; a USB 3.0 controller, on the other hand, waits for a device to raise an “attention needed” flag before waking up and acknowledging the request; other devices on the bus remain in a quiescent state while the host and device complete their transaction. USB 3.0 also implements link power management, which further reduces power consumption.

» View Featured Interface Products for Low Power

Texas Instruments LMZ217xx SIMPLE SWITCHER® Nano Modules
Texas Instruments
LMZ217xx
SIMPLE SWITCHER® Nano Modules

LMZ217xx SIMPLE SWITCHER® Nano Modules are an easy-to-use, step-down DC-DC solution that are capable of driving up to 1000mA load in point-of-load and other space-constrained applications.
Learn more about Texas Instruments LMZ217xx SIMPLE SWITCHER® Nano Modules
Fairchild N-Channel PowerTrench® MOSFETs: Extended Temperature
Fairchild N-Channel
PowerTrench® MOSFETs:
Extended Temperature

Available in a thermally efficient MicroFET Package, N-Channel PowerTrench® MOSFETs have been tailored to minimize on-state resistance, provide superior switching performance, plus withstand high energy pulse in avalanche and commutation modes.
Learn more about Fairchild N-Channel PowerTrench® MOSFETs: Extended Temperature
ON Semiconductor NCP103 150 mA CMOS Low Dropout Regulators
ONSemiconductor NCP103
150 mA CMOS Low Dropout Regulators


NCP103 Low Dropout Regulators are a 150mA LDO that employs a dynamic quiescent current adjustment for very low IQ consumption at no−load, plus provides a very stable, accurate voltage with low noise suitable for space constrained, noise sensitive applications.
Learn more about ON Semiconductor NCP103 150 mA CMOS Low Dropout Regulators
STMicroelectronics STGAP1S gapDRIVE™ Gate Drivers
STMicroelectronics
STGAP1S gapDRIVE™
Gate Drivers

The STGAP1S gapDRIVE™ is a 5A galvanically isolated single-gate driver for N-channel MOSFETs and IGBTs with advanced protection, configuration and diagnostic features.
Learn more about STGAP1S gapDRIVE™ Gate Drivers
Maxim Integrated MAX14692/MAX14693 High-Accuracy Adjustable Power Limiters
Maxim Integrated
MAX14692/MAX14693 High-Accuracy
Adjustable Power Limiters

MAX14692/MAX14693 High-Accuracy Adjustable Power Limiters are adjustable overvoltage, undervoltage and overcurrent protection devices that guard systems against overcurrent faults in addition to positive overvoltage and reverse-voltage faults.
Learn more about Advantech MIO-5250 3.5 in. MIO-Compact SBC
Vishay SiC620 Integrated DrMOS Power Stages
Vishay SiC620
Integrated DrMOS Power Stages


The SiC620 DrMOS Power Stages are an integrated solution that deliver industry benchmark performance by significantly reducing switching and conduction losses and are optimized for synchronous buck applications.
Learn more about Vishay SiC620 Integrated DrMOS Power Stages
More Featured Products
Semiconductors
Maxim Integrated - MAX44264 Ultra-Small Op AmpsLearn More
Microchip Technology - nanoWatt XLP™ TechnologyLearn More
NXP - LPC800 Cortex-M0+ 32-Bit MCUsLearn More
RF Modules
Panasonic - Bluetooth RF ModulesLearn More