Contact Mouser (International)  +49 (0)89 520 462 110     |     Feedback         
    
Cart  
 |    Change Country  Change Location  USD
 
Mouser International Mouser International

Incoterms: DDP is available to customers in EU Member States.
All prices include duty and customs fees on select shipping methods.


Incoterms: DDU applies to most non-EU customers.
Duty, customs fees and taxes are collected at time of delivery.

Please confirm your currency selection:

US Dollars
USD is accepted in all countries.

Other currency options may also be available - see
Mouser Worldwide.
Home » Applications & Technologies » Smart Grid Technology Electronics
Applications & Technologies
Smart Grid

“Smart grid” is a term recognized now in many circles, but why exactly does the grid need to be smarter? For one, the current power grid has trouble matching power supply and demand, wasting energy or leading to outages. Power must be generated from a relatively small number of very large facilities, and in quantities that meticulously fit the predicted load curve. This problem stems partly from the fact that the grid was built to facilitate only unidirectional flow of power and control – a topology that is increasingly more costly to maintain. This means that today’s infrastructure is not only less efficient and less robust, but it is also incapable of incorporating a significant amount of renewable and non-dispatchable energy sources into the grid.

Viewed at its highest level, the smart grid can be understood as any and all technologies, standards, and practices that contribute to a more efficient and more reliable power grid. Simply enabling greater consumer participation can accomplish much of this, and is an overarching goal of smart grid. Dynamic energy pricing allows consumers to adjust when and how high-load devices are used, ultimately lowering energy bills and reducing the demand spikes which can lead to power outages. A smart appliance can even do this automatically, optimizing its operation to minimize cost and waste – a feature of smart grid called “prices-to-devices”.

Smart grid technology promises this and many additional methods for reducing waste, lowering peak demand, improving grid reliability, and integrating renewable resources. The roll-out of smart meter devices has been significant and smart grid technology continues to gain momentum with each new innovation. The power grid may have been created "dumb", but Mouser Electronics offers the newest products and tools to help raise its IQ.

» Learn More About Smart Grid

Smart Meter

By today's technological standards, the common electromechanical energy meter is a relic of the past – incapable of anything but flat-rate pricing and infrequent meter readings.

Smart meters go well beyond the rudimentary functions of a basic electrical meter. Above all, the distinguishing quality of a smart meter is to support 2-way communication with utility providers. This is the key that opens the door to all other "smart" functions and the benefits thereof. Smart meters can provide support for remote diagnostics, dynamic pricing, tamper notification, consumption analysis, and more.

What does this mean for utility customers? For one, it creates something that has not existed since the grid's creation: an informed consumer base. People can analyze their own energy usage in as much detail as desired and then adjust the amount, manner, and time in which high load devices are used. Even today, most consumers are unaware that for utility providers, the cost of a kWh is greater during times of peak demand – after all, electricity is traditionally billed at a flat rate. By offering dynamic pricing based on real-time energy demand, electric companies create opportunities for customers to significantly lower their energy bill with simple changes, such as using the clothes dryer at off-peak hours. Also, these kinds of changes have the effect of reducing or "shaving" the demand peaks over the course of a day, which can further reduce energy costs.

» Learn More about Smart Meters

Smart Home

Smart Home GatewaysSmart Meter solutions such as Automated Meter Reading (AMR) and Advanced Metering Infrastructure (AMI), along with smart appliances, provide many benefits to utility companies and their customers. Customers become empowered by controlling these devices via remote computer or smart phone. For utility companies this adds a level of service that includes outage detection, better demand response, more flexible billing cycles, remote meter control, more accurate readings, and reduced time needed for manual data collection. Using smart meter solutions allows utility companies to avoid outdated methods for calculating energy usage at each residence.

Smart Appliances

» Wifi/WiMaxBluetooth

» RF Whip/Chip Antenna

» RF Connectors

» MCUs

» Motion Sensors

» Temperature Sensors

Wireless Gateways

» Gateways

» RF Whip/Chip Antenna

» RF Connectors

Test & Tools

Kits & Demo BoardsSmart Grid represents a spectrum of rapidly evolving technologies. As design complexity increases and design cycles continue to shrink, development tools are often all but essential. In the area of Smart Meter, development kits and boards provide designers the means to evaluate and become familiar with the latest Smart Grid products.

ToolsIn addition to accelerated time-to market, development kits can further provide the benefits of directly applicable, pre-tested circuits, readily available printed circuit board (PCB) layouts, and a common platform from which to create and debug customized designs.

The often iterative process of design must include development and testing beyond mere circuit simulation. Test and Measure equipment like oscilloscopes help engineers shorten the process by allowing multiple measurements across various ICs being used.

Test Equipment

» Oscilloscopes and Accessories

Tools

» Radio Development Kits

» PLC Development Kits

» In Home Tool Development Kits

» MCU Development Kits

» E-Meter IC Development Kits

» Power IC Development Kits

» Anti-Tamper Development Kits

Texas Instruments CC26xx SimpleLink Ultra-Low Power Wireless Microcontrollers
Texas Instruments
CC26xx SimpleLink Ultra-Low
Power Wireless Microcontrollers

Wireless MCUs that target Bluetooth® Smart, ZigBee and 6LoWPAN, and ZigBee RF4CE remote control applications. These cost-effective, ultra-low power, 2.4-GHz RF devices offer very low active RF and MCU current, and low-power mode current consumption.
Learn more about Texas Instruments CC26xx SimpleLink Ultra-Low Power Wireless Microcontrollers
Molex Standalone Antennas
Molex
Standalone Antennas


Global smart grid deployments are leading in M2M (machine-to-machine) wireless communication. Molex antennas deliver superior performance for less cost and risk—and shortened lead times for bringing wireless products to market.
Learn more about Molex Standalone Antennas
Murata AMR Sensors (Magnetic Switches)
Murata
AMR Sensors (Magnetic Switches)


Exploiting the magnetoresistive effect, AMR sensors have an IC to detect changes in the magnetic resistance of a magnetoresistive element affected by an external magnetic field. Many magnetic switches are used for cylinder position detection, robotics, smart meter, and open/close detection.
Learn more about Murata AMR Sensors (Magnetic Switches)
Amphenol RF/Connex MCX Series Connectors
Amphenol
RF/Connex MCX Series Connectors


Exhibiting a maximum frequency of up to 6GHz Amphenol RF's line of MCX (micro coaxial) connectors and adapters exhibit broadband performance with low reflection. They feature quick connect/disconnect snap-on mating and have smaller outer diameters than SMB (Subminiature version B) connectors.
Learn more about Amphenol RF/Connex MCX Series Connectors
Omron G5RL-U/-K PCB Power Relay
Omron
G5RL-U/-K PCB Power Relay


Omron G5RL-U/-K PCB Power Relays are available in Single coil or Dual coil latching models and feature creepage distance of 8mm between coil and contacts, an ambient operating temperature of 85°C, and TV-8 rating (1FormA models).
Learn more about Omron G5RL-U/-K PCB Power Relay
Cypress Serial F-RAM Nonvolatile Memory Devices
Cypress
F-RAM Nonvolatile
Memory Devices

These memories combine the nonvolatile data storage capability of ROM with the fast speeds of RAM. Serial F-RAM features a variety of interface and density options, including SPI and I²C interfaces, industry-standard packages, and densities ranging from 4-kilobit to 2-megabit.
Learn more about Cypress Serial F-RAM Nonvolatile Memory Devices
More Featured Products
Wireless
Laird Wireless - LT1110 915 MHz Wireless ModulesLearn More
Molex - 47950 Series 2.4/5 GHz WIFI AntennasLearn More
Memory
Greenliant - NANDrive™ GLS85 Series Embedded Solid State DrivesLearn More
Everspin Technologies - MRAM Memory ProductsLearn More
Passive Components
EPCOS - B82804A Series Gate Drive TransformersLearn More
AVX - BestCap® Pulse SupercapacitorsLearn More
Test & Measurement
LeCroy - WaveSurfer® OscilloscopesLearn More
Connectors
Amphenol - Micro Miniature Coaxial (AMMC) Connectors and Jumper CablesLearn More
3M - Power Clamp ConnectorsLearn More